Method (Write Only)
SCPI.MMEMory.STORe.PLIMit = File
This command saves the point limit table of the active trace of the active channel into a file in the CSV format (extension ".csv").
This command is available at the revision A.11.0x and above.
Specify the file name with the extension. When you use directory names and file name, separate them with "\ " (back slash), or "/" (slash).
|
Parameter |
File |
|
Description |
File name to save the point limit table (extension ".csv") |
|
Data type |
Character string type (String) |
|
Range |
254 characters or less |
|
Note |
If a file with the same name as the specified file name exists, its contents are overwritten. |
SCPI.DISPlay.WINDow(1).ACTivate
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.MMEMory.STORe.PLIMit = "d:\plimit01.csv"
SCPI.DISPlay.WINDow(1).ACTivate
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.MMEMory.STORe.PLIMit = "test/plimit01.csv"
SCPI.DISPlay.WINDow(Ch).ACTivate
SCPI.CALCulate(Ch).PARameter(Tr).SELect
Analysis > Point Limit Test > Edit Point Limit > Export to CSV File...
:MMEMory:STORe:PLIMit <string>
10 OUTPUT 717;":MMEM:STOR:PLIM ""Test1/PLimit01.csv"""
10 OUTPUT 717;":MMEM:STOR:PLIM ""D:\PLimit01.csv"""