Property (Read-Write)
SCPI.SENSe(Ch).SEGMent.LIST.POWer.PORT.STATe = Status
Status = SCPI.SENSe(Ch).SEGMent.LIST.POWer.PORT.STATe
This command turns ON/OFF the individual (Port 1, Port 2 or Port 4) power control in the segment sweep table. This command is supported in revision A.11.20 and above.
|
Parameter |
Status |
|
Description |
ON/OFF the individual port power control |
|
Data type |
Boolean type (Boolean) |
|
Range |
Select from either of the following:
|
|
Preset value |
False or OFF |
Dim SegmState As Boolean
SCPI.SENSe(1).SEGMent.LIST.POWer.PORT.STATe = True
SegmState= SCPI.SENSe(1).SEGMent.LIST.POWer.PORT.STATe
SCPI.SENSe(Ch).SEGMent.LIST.CONTrol.DATA
SCPI.SENSe(Ch).SEGMent.LIST.CONTrol.STATe
SCPI.SENSe(Ch).SEGMent.LIST.POWer.PORT(Pt).LEVel.IMMediate.AMPLitude
Sweep Setup > Edit Segment Table > List Port Power > ON|OFF
:SENSe{[1]-160}:SEGMent:LIST:POWer:PORT:STATe {ON|OFF|1|0}
:SENSe{[1]-160}:SEGMent:LIST:POWer:PORT:STATe?
{1|0}<newline><^END>
10 OUTPUT 717;":SENS1:SEGMent:LIST:POWer:PORT:STATe ON"
20 OUTPUT 717;":SENS1:SEGMent:LIST:POWer:PORT:STATe?"
30 ENTER 717;A