Property (Read-Write)
SCPI.SENSe(Ch).FREQuency.STARt = Value
Value = SCPI.SENSe(Ch).FREQuency.STARt
This command sets/gets the start value of the sweep range of selected channel (Ch).
|
Parameter |
Value |
|
Description |
Start value |
|
Data type |
Double precision floating point type (Double) |
|
Range |
|
|
Preset value |
1E5 |
|
Unit |
Hz (hertz) |
|
Resolution |
1 |
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
Dim Start As Double
SCPI.SENSe(1).FREQuency.STARt = 100E6
Start = SCPI.SENSe(1).FREQuency.STARt
Start
:SENSe{[1]-160}:FREQuency:STARt <numeric>
:SENSe{[1]-160}:FREQuency:STARt?
{numeric}<newline><^END>
10 OUTPUT 717;":SENS1:FREQ:STAR 100E6"
20 OUTPUT 717;":SENS1:FREQ:STAR?"
30 ENTER 717;A