Property (Read-Write)
SCPI.SENSe(Ch).SEGMent.SLOCal.STATe = Status
Status = SCPI.SENSe(Ch).SEGMent.SLOCal.STATe
This command turns ON/OFF the individual Shift LO state control in the segment sweep table.
|
Parameter |
Status |
|
Description |
ON/OFF of the individual Shift LO state control |
|
Data Type |
Boolean type (Boolean) |
|
Range |
Select from either of the following: True or ON: Turns ON the individual Shift LO state control. False or OFF: Turns OFF the individual Shift LO state control. |
|
Preset Value |
OFF or 0 |
Dim SegmData As Variant
SCPI.SENSe(1).SEGMent.DATA = Array(6,0,1,0,0,1,0,2, _
100E6,2E9,31,70E3,2,2E9,3E9,101,300E3,3)
SegmData = SCPI.SENSe(1).SEGMent.DATA
Dim SegmState As Boolean
SCPI.SENSe(1).SEGMent.SLOCal.STATe = True
SegmState= SCPI.SENSe(1).SEGMent.SLOCal.STATe
SCPI.SENSe(Ch).SEGMent.SLOCal.DATA
Sweep Setup > Edit Segment Table > List Shift LO > ON|OFF
:SENSe{[1]-160}:SEGMent:SLOCal:STATe {ON|OFF|1|0}
:SENSe{[1]-160}:SEGMent:SLOCal:STATe?
{1|0} <newline><^END>
10 DIM H(1:2,1:5)
20 OUTPUT 717;":SENS1:SEGM:DATA 6,0,1,0,0,1,0,2,";
30 OUTPUT 717;"100E6,2E9,31,70e3,2,";
40 OUTPUT 717;"2E9,3E9,101,300e3,3"
50 OUTPUT 717;":SENS1:SEGM:DATA?"
60 ENTER 717;A,B,C,D,E,F,G,H(*)
10 OUTPUT 717;":SENS1:SEGMent:SLOCal:STATe ON"
20 OUTPUT 717;":SENS1:SEGMent:SLOCal:STATe?"
30 ENTER 717;A