Property (Read-Write)
SCPI.SOURce(Ch).POWer.ATTenuation.AUTO = Status
Status = SSCPI.SOURce(Ch).POWer.ATTenuation.AUTO
This command turns on/off the Auto Power Range set function for the channels (Ch).
When the Auto Power Range set function is ON, the minimum value of step attenuation is selected according to the available source power range as described below:
|
Source Power Range |
Step Attenuation |
|
-25 ~ +10 dBm |
0 dB |
|
-35 ~ -25 dBm |
10 dB |
|
-45 ~ -35 dBm |
20 dB |
|
-55 ~ -45 dBm |
30 dB |
|
-65 ~ -55 dBm |
40 dB |
|
-75 ~ -65 dBm |
50 dB |
|
-85 ~ -75 dBm |
60 dB |
The power sweep setting is set according to the start power level and maximum value of stop power level is set according to step attenuation. For more information on power attenuation, refer to Setting Power Level with Auto Power Range.
This command works only with the E5071C options 2D5, 4D5, 2K5 and 4K5 having a mechanical source attenuator. This command is neither required nor available in other E5071C options which are having electrical source attenuator and is provided to maintain backward compatibility.
|
Parameter |
Status |
|
Description |
Dummy Parameter |
|
Data type |
Boolean type (Boolean) |
|
Range |
Select from either of the following:
|
|
Preset value |
True or ON |
SCPI.SOURce(Ch).POWer.ATTenuation.DATA
Sweep Setup > Power > Auto Range
:SOURce{[1]-160}:POWer:ATTenuation:AUTO {ON|OFF|1|0}
:SOURce{[1]-160}:POWer:ATTenuation:AUTO?
{1|0}<newline><^END>
10 OUTPUT 717;":SOUR1:POW:ATT:AUTO ON"
20 OUTPUT 717;":SOUR1:POW:ATT:AUTO?"
30 ENTER 717;A