Property (Read-Write)
SCPI.SOURce(Ch).POWer.LEVel.IMMediate.AMPLitude = Value
Value = SCPI.SOURce(Ch).POWer.LEVel.IMMediate.AMPLitude
This command sets/gets the power level of the selected channel (Ch).
|
Parameter |
Value |
|
Description |
Power level |
|
Data type |
Double precision floating point type (Double) |
|
Range |
Varies depending on the power range. |
|
Preset value |
0 |
|
Unit |
dBm |
|
Resolution |
0.05 |
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
Dim PowLev As Double
SCPI.SOURce(1).POWer.LEVel.IMMediate.AMPLitude = -10
PowLev = SCPI.SOURce(1).POWer.LEVel.IMMediate.AMPLitude
SCPI.SOURce(Ch).POWer.ATTenuation.DATA
SCPI.SOURce(Ch).POWer.ATTenuation.AUTO
Sweep Setup > Power
:SOURce{[1]-160}:POWer[:LEVel][:IMMediate]
[:AMPLitude] <numeric>
:SOURce{[1]-160}:POWer[:LEVel][:IMMediate]
[:AMPLitude]?
{numeric}<newline><^END>
10 OUTPUT 717;":SOUR1:POW -12.5"
20 OUTPUT 717;":SOUR1:POW?"
30 ENTER 717;A