Property (Read-Write)
SCPI.SYSTem.COMMunicate.PSENsor = <char>,<string>
Param = SCPI.SYSTem.COMMunicate.PSENsor
This command specifies the type and location of the power meter to be used in a source power calibration
|
Parameter |
char |
|
Description |
Power Meter Type |
|
Data type |
Character string type (String) |
|
Range |
Select from either of the following:
|
|
Parameter |
string |
|
Description |
Address/ID string of Power Meter |
|
Data type |
Character string type (String) |
|
Range |
For char=GPIB, address of the power meter. Choose any integer between 0 and 30. For char=USB, the ID string of the power meter or power sensor. Use SYST:COMM:USB:PMET:CAT? to see a list of ID strings of connected power meters and sensors. |
Dim PsenModel As String
PsenModel = SCPI.SYSTem.COMMunicate.USB.PMETer.CATalog
SCPI.SYSTem.COMMunicate.PSENsor = Array("USB", PsenModel)
SYSTem.COMMunicate.USB.PMETer.CATalog
System > Misc Setup > Power Meter Setup > Select Type > GPIB|USB
:SYSTem:COMMunicate:PSENsor {GPIB|USB},{string (address/ID string)}
:SYSTem:COMMunicate:PSENsor?
{GPIB|USB},{string (address/ID string)}<newline><^END>
10 OUTPUT 717;":SYST:COMM:USB:PMET:CAT?"
20 ENTER 717;A$
30 OUTPUT 717;":SYST:COMM:PSEN USB,"&A$