Property (Read-only)
Ctlg = SCPI.SYSTem.COMMunicate.USB.PMETer.CATalog
This command reads the ID string of power meters / sensors that are connected to the ENA through USB. Use the list to select a power sensor for a source power cal.
| 
 Parameter  | 
 Ctlg  | 
| 
 Description  | 
 Returns a string containing the following parameters for all the connected power meters/sensors: 
  | 
| 
 Data type  | 
 Character string type (String)  | 
Dim Ctlg As String
Ctlg = SCPI.SYSTem.COMMunicate.USB.PMETer.CATalog
SCPI.SYSTem.COMMunicate.PSENsor
No equivalent key is available on the front panel.
:SYSTem:COMMunicate:USB:PMETer:CATalog
{string}<newline><^END>
10 OUTPUT 717;":SYSTem:COMMunicate:USB:PMETer:CATalog?"
20 ENTER 717;A$