Method (Write-only)
SCPI.TRIGger.SEQuence.IMMediate
This command generates a trigger immediately and executes a measurement, regardless of the setting of the trigger mode.
This command is different from SCPI.TRIGger.SEQuence.SINGle as the execution of the object finishes at the time of a trigger.
If you execute this object when the trigger system is not in the trigger wait state (trigger event detection state), an error occurs when executed and the object is ignored.
SCPI.TRIGger.SEQuence.SOURce = "bus"
SCPI.INITiate(1).CONTinuous = True
SCPI.TRIGger.SEQuence.IMMediate
SCPI.TRIGger.SEQuence.IMMediate
No equivalent key is available on the front panel.
:TRIGger[:SEQuence][:IMMediate]
10 OUTPUT 717;":TRIG:IMM"
20 OUTPUT 717;"*OPC?"
30 ENTER 717;A