Property (Read-Write)
SCPI.TRIGger.SEQuence.POINt = Status
Status = SCPI.TRIGger.SEQuence.POINt
This command turns ON/OFF or returns the status of the point trigger feature.
When the point trigger feature is turned on, if the sweep mode is Swept, it changes to Stepped.
When the trigger source is set to the internal trigger (Internal), the setting is ignored.
|
Parameter |
Status |
|
Description |
Turns ON/OFF the point trigger |
|
Data type |
Boolean type (Boolean) |
|
Range |
Select from either of the following: True or ON: Turns on the point trigger. False or OFF: Turns off the point trigger. |
|
Preset value |
False or OFF |
|
Note |
|
Dim Ptrig As Boolean
SCPI.TRIGger.SEQuence.POINt = True
Ptrig = TRIGger.SEQuence.POINt
Trigger > Trigger Event
:TRIGger[:SEQuence]:POINt {ON|OFF|1|0}
:TRIGger[:SEQuence]:POINt?
{1|0}<newline><^END>
10 OUTPUT 717;":TRIG:POIN ON"
20 OUTPUT 717;":TRIG:POIN?"
30 ENTER 717;A