Differential Matching Circuit Embedding (only 3-port/4-port models)
Differential Port Impedance Conversion (only 3-port/4-port models)
Other topics about Analyzing Data
The Fixture Simulator provides the following functions:
Matching Circuit Embedding
Port Impedance Conversion
Network De-embedding
4-Port Network Embedding/De-embedding
Balance-Unbalance Conversion (only 3-port/4-port models)
Differential Matching Circuit Embedding (only 3-port/4-port models)
Differential Port Impedance Conversion (only 3-port/4-port models)
Before you can use any of the features listed above, you must turn on the desired feature individually and issue the following command to turn on the Fixture Simulator:
:CALC{1-36}:FSIM:STATThe Matching Circuit feature simulates the characteristics that the DUT would exhibit when connected to a matching circuit.
To turn on or off the Matching Circuit, use the following command:
:CALC{1-36}:FSIM:SEND:PMC:STAT
You can only turn on or off Matching Circuit for all the ports, not for each port individually. However, any port whose circuit type is set to "None" behaves as if this feature were permanently off.
To select a circuit type, use the following command:
:CALC{1-36}:FSIM:SEND:PMC:PORT{1-4}
To set the circuit constant, use the following commands:
|
Circuit constant |
Command |
|
C |
:CALC{1-36}:FSIM:SEND:PMC:PORT{1-4}:PAR:C |
|
G |
:CALC{1-36}:FSIM:SEND:PMC:PORT{1-4}:PAR:G |
|
L |
:CALC{1-36}:FSIM:SEND:PMC:PORT{1-4}:PAR:L |
|
R |
:CALC{1-36}:FSIM:SEND:PMC:PORT{1-4}:PAR:R |
When you want to use a user file to define the circuit type, specify the file by using the following command:
:CALC{1-36}:FSIM:SEND:PMC:PORT{1-4}:USER:FIL
The Port Impedance Conversion feature converts the measurement results with a port impedance of 50 ohm to the characteristics of a different port impedance.
To turn on or off Port Impedance Conversion, use the following command:
:CALC{1-36}:FSIM:SEND:ZCON:STAT
You can only turn on or off Port Impedance Conversion for all of the ports, not for each port individually. However, any port with ZO set to 50 ohm behaves as if this feature were permanently off.
To set the target port impedance, use the following command:
:CALC{1-36}:FSIM:SEND:ZCON:PORT{1-4}:Z0
:CALC{1-36}:FSIM:SEND:ZCON:PORT{1-4}:REAL
:CALC{1-36}:FSIM:SEND:ZCON:PORT{1-4}:IMAG
The Network De-embedding feature eliminates any network that can cause error between the calibration level and the DUT.
To turn on or off Network De-embedding, use the following command:
:CALC{1-36}:FSIM:SEND:DEEM:STAT
You can only turn on or off Network De-embedding for all of the ports, not for each port individually. However, any port whose Network De-embedding type is set to "None" behaves as if this feature were permanently off.
To select a Network De-embedding type, use the following command:
:CALC{1-36}:FSIM:SEND:DEEM:PORT{1-4}
To specify the file that defines the criteria for Network De-embedding, use the following command:
:CALC{1-36}:FSIM:SEND:DEEM:PORT{1-4}:USER:FIL
The 4-port Network Embedding/De-embedding feature is provided to embed or de-embed a network (defined in a 4-port touchstone file) between the calibration surface and the DUT.
To turn on or off the 4-port network embedding/de-embedding feature, use the following command:
:CALC{1-36}:FSIM:EMB:STAT
To select a connection type, use the following command:
:CALC{1-36}:FSIM:EMB:TYPE

To assign the ports (ports a through d in Connection_type), use the appropriate command that matches your selected connection type, as identified in the following table:
|
Connection type |
Command |
|
A |
:CALC{1-36}:FSIM:EMB:TOP:A:PORT |
|
B |
:CALC{1-36}:FSIM:EMB:TOP:B:PORT |
|
C |
:CALC{1-36}:FSIM:EMB:TOP:C:PORT |
To select a network processing type, use the following command:
:CALC{1-36}:FSIM:EMB:NETW{1-2}:TYPE
To select a file that defines the criteria for network embedding/de-embedding, use the following command:
:CALC{1-36}:FSIM:EMB:NETW{1-2}:FILThe Balance-Unbalance Conversion feature converts the measurement results obtained in an unbalanced state to the characteristics of a balanced state. You can select mixed mode S parameter, balance and CMRR as the measurement parameter when you turn on Balance-Unbalance Conversion.
You can turn on or off Balance-Unbalance Conversion for each trace individually. To turn on or off Balance-Unbalance Conversion, use the following command:
:CALC{1-36}:FSIM:BAL:PAR{1-36}:STAT
To select a balance device type, use the following command:
:CALC{1-36}:FSIM:BAL:DEV

To assign the ports (ports a through d in Balance_device_type), use the command that matches your selected device type, as identified in the following table:
|
Device Type |
Command |
|
Unbalance-balance (SBALanced) |
:CALC{1-36}:FSIM:BAL:TOP :SBAL |
|
Balance-balance (BBALanced) |
:CALC{1-36}:FSIM:BAL:TOP :BBAL |
|
Unbalance-unbalance-balance (SSBalanced) |
:CALC{1-36}:FSIM:BAL:TOP :SSB |
To select the measurement parameter, use the command that matches your selected device type, as identified in the following table:
|
Device Type |
Command |
|
Unbalance-balance |
:CALC{1-36}:FSIM:BAL:PAR{1-36} :SBAL |
|
Balance-balance |
:CALC{1-36}:FSIM:BAL:PAR{1-36} :BBAL |
|
Unbalance-unbalance-balance |
:CALC{1-36}:FSIM:BAL:PAR{1-36} :SSB |
The Differential Matching Circuit Embedding feature simulates the characteristics the DUT would exhibit if a balance-unbalance converted differential port were connected to a matching circuit after being subjected to balance-unbalance conversion.
To turn on or off Differential Matching Circuit Embedding, use the following command:
:CALC{1-36}:FSIM:BAL:DMC:STAT
You can only turn on or off Differential Matching Circuit Embedding for all of the ports, not for each balance port individually. However, any balance port whose circuit type is set to "None" behaves as if this feature were permanently off.
To select a circuit type, use the following command:
:CALC{1-36}:FSIM:BAL:DMC:BPOR{1-2}
To set the circuit constant, use the following commands:
|
Circuit constant |
Command |
|
C |
:CALC{1-36}:FSIM:BAL:DMC:BPOR{1-2}:PAR:C |
|
G |
:CALC{1-36}:FSIM:BAL:DMC:BPOR{1-2}:PAR:G |
|
L |
:CALC{1-36}:FSIM:BAL:DMC:BPOR{1-2}:PAR:L |
|
R |
:CALC{1-36}:FSIM:BAL:DMC:BPOR{1-2}:PAR:R |
When you want to use a user file to define the circuit type, specify the file using the following command:
:CALC{1-36}:FSIM:BAL:DMC:BPOR{1-2}:USER:FIL
The Differential Port Impedance Conversion feature converts the measurement results for a balance-unbalance converted differential port to the characteristics of a different port impedance.
To turn on or off Differential Port Impedance Conversion, use the following command:
:CALC{1-36}:FSIM:BAL:DZC:STAT
You can only turn on or off Differential Port Impedance Conversion for all of the balance ports, not for each port individually.
To set the target differential port impedance, use the following command:
:CALC{1-36}:FSIM:BAL:DZC:BPOR{1-2}:Z0
:CALC{1-36}:FSIM:BAL:DZC:BPOR{1-2}:REAL
:CALC{1-36}:FSIM:BAL:DZC:BPOR{1-2}:IMAG
See Fixture Simulator.