Partial Overwrite

Other topics about Performing Calibration

Overview

The E5071C has the following calibration coefficients for full N-port calibration: Er, Es, Ed (reflection), Et (transmission), and Ex (isolation).The partial overwrite function is used to measure some of these calibration coefficients after completion of the initial calibration and then to overwrite them.

The conditions under which the calibration coefficients can be calculated by the partial overwrite are as follows:

If calculation of the calibration coefficients is attempted without the measurements required to execute the partial overwrite, an error message (20: Additional Standard Needed) is displayed.

Executing calculation of calibration coefficients using partial overwrite

To calculate the calibration coefficients using partial overwrite, use the following command:

:SENS{1-36}:CORR:COLL:PART:SAVE