Query Only
:CALCulate:EYE:RESults:DATA?
This command returns the results of eye measurement. The 18 values are returned. The minimum and maximum values are returned in addition of the displayed results (16 values) on the TDR application GUI.
|
Description |
Results of eye measurement |
|
Data Type |
Variant type Array (Range) |
|
Range |
- |
|
Preset Value |
- |
|
Unit |
- |
|
Resolution |
- |
{numeric (Minimum Value)},{numeric (Maximum Value)},{numeric (Level Zero)},{numeric (Level One)}, {numeric (Level Mean)},{numeric (Amplitude)},{numeric (Height)},{numeric (always 0)}, {numeric (Width)},{numeric (Opening Factor)}, {numeric (Signal/Noise Ratio)}, {numeric (Duty Cycle Distortion)},{numeric (Duty Cycle Distortion-%)},{numeric (Rise Time)},{numeric (Fall Time)},{numeric (Jitter peak to peak)},{numeric (Jitter RMS)},{numeric (Crossing Percentage)}<newline><^END>
10 OUTPUT 717;":CALC:EYE:STAT ON"
20 OUTPUT 717 ":CALC:ATR:ACT 3"
30 OUTPUT 717;":CALC:EYE:RES:THR T2_8"
30 OUTPUT 717;":CALC:EYE:EXEC"
40 OUTPUT 717;":CALCulate:EYE:RESults:DATA?"
50 ENTER 717;A(*)
:CALCulate:EYE:RESults:THReshold
Eye Mask > Result Window (Under Result)
Eye Mask > Export to CSV (Under Result)
(Not exactly equivalent)