Command Only
:SENSe:CORRection:COLLection:DLComp:THRU
This command executes a thru measurement, as a part of Loss Compensation sequence.
Description |
Port number where the thru measurement is executed. |
Data Type |
Character string type (String) |
Range |
TH12: Thru between ports 1 and 2. TH13: Thru between ports 1 and 3. TH24: Thru between ports 2 and 4. |
Preset Value |
- |
Unit |
- |
Resolution |
- |
10 OUTPUT 717;":SENS:CORR:COLL:DLC:THRU TH12"
20 OUTPUT 717; ":SENS:CORR:COLL:DLC:SAVE"
:SENSe:CORRection:COLLection:DLComp:OPEN
:SENSe:CORRection:COLLection:DLComp:LOAD
:SENSe:CORRection:COLLection:DLComp:SAVE
Setup > Deskew & Loss Compensation (under Basic) > Measure