Other topics about Setting Control Functions
The serial number and options of the E5071C can be checked using the following procedure.
Press System > Firmware Revision.
The Firmware Revision dialog which shows the serial number and options is displayed.
The information of MWA option is not displayed here as the MWA software is a VBA macro.
To activating software option, see Activating Software Option.
The revision number and system information of the firmware installed in the E5071C can be checked using the following procedure.
Press System > Firmware Revision.
The Firmware Revision dialog is displayed, as shown below.

Click on the PC Info button to view System Properties.

Press System > Firmware Revision.
The Firmware Revision dialog which shows the HDD revision is displayed.
In firmware older than revision A.09.7x, the HDD revision is not displayed at the Firmware Revision dialog box.
The HDD revision of the E5071C can be checked using Windows Start Menu > My Computer > C: drive label. For example, the HDD version of the E5071C in the figure below is CN920. For more information, refer to HDD Revision History.