Show 

Connecting External Accessories

The E5071C can be connected to external input/output devices such as printer, monitor, keyboard and mouse using any of the serial or USB ports provided in the rear or the front panel.

Other topics about Using Windows

Connecting a Printer

A printer can be connected to the E5071C using the Universal Serial Bus (USB) ports provided in the front or rear panel.

Connecting a Mouse

A mouse can be connected to the E5071C through the Universal Serial Bus (USB) ports provided in the front or rear panel.

Connecting a Monitor

A monitor can be connected to the E5071C using the External Monitor Output Terminal (Video) located in the rear panel of the E5071C.

Connecting a Keyboard

A keyboard can be connected to the E5071C through the Universal Serial Bus (USB) ports provided in the front or rear panel.