Ripple Test

Other topics about Data Analysis

Overview

Independently of the limit test, you can evaluate the measurement results on a pass/fail basis by setting a limit for the ripple. This function is called the ripple test.

Concept of Ripple Test

The ripple test is a function for evaluating the results on a pass/fail basis based on the ripple limit, which is set using the ripple limit table. You can specify up to 12 frequency bands, which permits a test for each frequency band.

The ripple test judges the measurement as "Pass" when the ripple value specified with the ripple limit is not exceeded by any of the measurement points on the trace; otherwise, it judges the measurement as "Fail." For the measurement points in a stimulus range without a specified ripple limit, the test judges the measurement as "Pass."

The ripple limit is defined with the start point stimulus value, end point stimulus value, ripple limit value, and type (ON/OFF). For detailed information, see Configuring ripple limit.

While the ripple test function is turned ON, the measurement points corresponding to a "fail" judgment will be indicated in red on the screen, and the trace's test results based on the results of each measurement point will be displayed (judged as "fail" if one or more red measurement point exist on the trace). For information on how to display the results, see Turning ON/OFF ripple test and displaying results. You can also confirm the channel test results on the screen (judged as "fail" if one or more failed traces appear in the limit test, ripple test, or bandwidth test within the channel).

 

Displaying Ripple Test Results

Measurement point and test results

Failed measurement points will be displayed in red on the screen. The test result for the trace is indicated as Pass or Fail in the upper-right area of the graph. You can also display the ripple value at the selected frequency band.

The result is displayed as Ripln:Pass (or Fail) for each trace. n denotes the trace number. Bn is followed by the ripple value (if the ripple display is turned OFF, only Bn is displayed without the ripple value).

For example, in the following figure, Ripl1:Pass in the first line indicates the result for Trace 1. The value following B3 is the ripple value at the third frequency band specified in the ripple test. Similarly, the second line indicates the test result for Trace 2, showing the ripple value at the first frequency band.

For information on how to display the results, see Turning ON/OFF ripple test and displaying results.

Test result for channel

If a channel has a judgment result of "fail," the message is displayed as shown in Test Result for Trace. (It is judged as failed if one or more failed traces are found in the limit test, ripple test, or bandwidth test within the channel.)

You can also specify the ON/OFF setting for the Fail Sign in the limit test menu as well as in the bandwidth test menu. From the ripple test menu, follow the steps below to turn it ON/OFF.

  1. Press Analysis.

  2. Click Ripple Limit > Fail Sign. This menu toggles between ON and OFF.

In addition to the screen, the following features also let you confirm the test results:

Configuring Ripple Limit

You must configure the ripple limit before you can use the ripple test function. You can specify a ripple limit table for each trace, where up to 12 ripple limit bands (frequency bands) can be configured.

Operational procedure

Follow the steps below to configure the ripple limits.

  1. Press Channel Next/Channel Prev and Trace Next/Trace Prev to select the trace of which you want to apply the ripple test function.

  2. Press Analysis to display the Analysis menu.

  3. Click Ripple Limit to display the softkeys for to the ripple test.

  4. Click Edit Ripple Limit to display the ripple limit table shown below.


  5. Create or edit the bands by using softkeys. Note that no frequency band is provided in the ripple limit table by default. The Edit Ripple Limit menu is also displayed, which can be used for creating or editing the frequency band.

  6. Click Add to add a frequency band to the ripple limit table and then specify the following parameters for the frequency band:
     

    Parameter

    Description

    Type

    Selects a frequency type, either ON or OFF.

    ON

    Band used for the ripple test.

    OFF

    Band not used for the ripple test.

    Begin Stimulus

    Specifies the start point for the stimulus value in the ripple test.

    End Stimulus

     

    Specifies the end point for the stimulus value in the ripple test.

    Max Ripple

    Specifies the ripple limit value.

  Example of ripple limit configuration

Saving/Recalling Ripple Limit Table

The ripple limit table can be saved in a file and recalled later for use on the screen. The file is saved in the csv format (with the extension *.csv), and values are saved as a character string with the unit. The csv formatted file can also be reused in spreadsheet software made for PCs.

Follow the steps below to save/recall the ripple limit table. This operation should be done by using the external keyboard and/or mouse.

  1. Display the ripple limit table.

  2. Click Export to CSV File from the Edit Ripple Limit menu to open the dialog box. At this time, CSV Files (with the extension *.csv) is selected as the file type.

  3. Specify any folder in which you want to save the file, and enter the file name. Click Save to save the ripple limit table displayed on the screen to a file.

  4. To recall the saved ripple limit table, click Import from CSV File from the Edit RippleLimit menu to display the Open dialog box. At this time, CSV File (with the extension *.csv) is selected as the file type.

  5. Specify the folder that contains the file, and then select the file. Click Open to recall the saved limit table on the screen.

  6. You can recall a limit table from a trace on any channel independently of the channel and trace that were active when the limit table was saved to the file.

The ripple limit table is saved in the following format:

Operational procedure

"# Channel 1"

"# Trace 1"

Type, Begin Stimulus, End Stimulus, MaxRipple

ON, 933.0000000 MHz, 964.0000000 MHz, 1.5 dB

ON, 938.0000000 MHz, 953.0000000 MHz, 500 mdB

ON, 953.0000000 MHz, 960.0000000 MHz, 300 mdB

Turning ON/OFF Ripple Test and Result Display

You can set the limit test ON/OFF for each trace individually.

  1. Press Channel Next/Channel Prev and Trace Next/Trace prev to select the trace for which you want to apply the ripple test function.

  2. Press Analysis to display the Analysis menu.

  3. Click Ripple Limit to display the softkeys for to the ripple test.

  4. Click the following corresponding softkeys.
     

    Softkey

    Function

    Ripple Test

    Sets the ripple test ON/OFF.

    Ripple Limit

    Sets the ripple limit line display ON/OFF.

    Ripple Value

    Sets how the ripple values are displayed. Available settings are turned OFF, absolute value (difference between maximum and minimum values within the band) display, and margin (difference between absolute value of ripple and ripple limit) display.

    Ripple Value Band

    Selects the band for which you want to display the ripple value.

    Edit Ripple Limit

    Opens the ripple limit table for editing the ripple limit. To use the ripple test function, you must first define the ripple limit.

Initializing Limit Table

The following operations initialize the limit table.