Overview of Fixture Simulator
Extending the Calibration Plane using Network De-embedding
Converting the Port Impedance of the Measurement Result
Determining Characteristics After Adding a Matching Circuit
Obtaining Characteristics After Embedding/De-embedding 4-port Network
Evaluating Balanced Devices (balance-unbalance conversion function)
Converting Reference Impedance of Balanced Port
Determining the Characteristics that Result from Adding a Matching Circuit to a Differential Port
Example of Using Fixture Simulator