Other topics about Making Measurement
The External Trigger Output port (located at the rear panel) can be used to provide trigger to an external device. This is useful in cases where an external device needs to be triggered through the E5072A.
Press Trigger key, and then click Ext Trig Output (1) > ON.

Click Polarity, and then select Positive Pulse or Negative Pulse (2).
|
Polarity Property |
Description |
|
Positive Pulse |
Generates a Positive Pulse as a trigger. |
|
Negative Pulse |
Generates a Negative Pulse as a trigger. |
Click Position, and then select After Point or Before Point (3).
|
Position Property |
Description |
|
After Point |
Generates a Pulse (trigger) after the measurement points. |
|
Before Point |
Generates a Pulse (trigger) before the measurement points. |
Difference between After and Before Point Settings
After and Before Point settings are shown as follows:

After Point:Pulse is generated after every measurement point.
Before Point:Pulse is generated before first measurement point. Rest of pulse are same timing as After Point. Number of pulse is same as number of measurement point.

After Point:Pulse is generated after every measurement point.
Before Point:Pulse is generated before every measurement point.