Expanding Dynamic Range

Other topics about Optimizing Measurement

Overview

The dynamic range is the finite difference between the maximum input power level and the minimum measurement power level (noise floor) of the analyzer. In evaluating a characteristic accompanied by a large change in the amplitude (the pass band and stop band of a filter, for example), it is important to increase the dynamic range.

Lowering Receiver Noise Floor

Lowering the noise floor of the receiver enables you to expand the dynamic range. The following methods can be used to lower the receiver noise floor.

Narrowing the IF bandwidth

Narrowing the receiver IF bandwidth enables you to reduce the effect of random noise on measurements. Narrowing the IF bandwidth to 1/10 the original bandwidth causes the receiver noise floor to decrease by 10 dB.

To specify the IF bandwidth, follow the steps described below.

  1. Press Channel Next/Channel Prev to select a channel on which to specify the IF bandwidth.

  2. Press Avg.

  3. Click IF Bandwidth, then  Change the IF bandwidth in the data entry area.

Turning on Sweep Averaging

Using sweep averaging also enables you to reduce the effects of random noise on measurements.

Sweep averaging averages data from each point (vector quantity) based on the exponential average of a continuous sweep weighted by the averaging factor specified by the user. Sweep averaging is expressed in following equation.

where:

Define the sweep averaging by following the steps below.

  1. Press Channel Next/Channel Prev to select the channel on which you want to define the sweep averaging.

  2. Press Avg.

  3. Click Avg Factor, then change the averaging factor in the data entry area.

  4. Click Averaging > ON.

  5. Clicking Averaging Restart resets n to 1 in Sweep Averaging equation in Turning on Sweep Averaging