Improving Phase Measurement Accuracy

This section describes the following functions that can be used to improve phase measurement accuracy.

Other topics about Optimizing Measurements

Electrical Delay

Electrical Delay is a function that adds or removes a pseudo-lossless transmission line with a variable length corresponding to the receiver input. Using this function enables you to improve the resolution in phase measurement and thereby measure deviation from the linear phase. You can specify the electrical delay trace by trace. Depending on the media type, different calculation methods for electrical delay are used to correct the phase delay.

  1. Press Channel Next/Channel Prev and Trace Next/Trace prev to select the active phase trace which you want.

  2. Press Scale.

  3. Click Electrical Delay.

  4. Change the electrical delay (in seconds) in the data entry area.

  5. Click Media, and select a media type for calculating the electrical delay. If the electrical delay is 0 second, the calculation result is always the same regardless of media type.
     

    Softkey   

    Function

    Coaxial

    Selects Coaxial as the media type.

    Waveguide

    Selects Waveguide as the media type.

  1. If you have selected Waveguide as the media type, click Cutoff Frequecy, and specify a cutoff frequency.

  2. The cutoff frequency is available only when the media type is Waveguide.

To determine the deviation from a linear phase, see Measuring the Deviation from a Linear Phase.

Procedure using marker

  1. Press Channel Next/Channel Prev and Trace Next/Trace prev to select the active phase trace which you want.

  2. Place the active marker in an appropriate position.

  3. Press Maker Fctn.

  4. Click Marker -> Delay to set the electrical delay (a value smoothed with the aperture of 20% regardless of the smoothing setting).

Phase offset

Phase offset is a function used to add or subtract a predetermined value relative to the frequency to and from the trace. Using this function enables you to simulate the phase offset occurring as a result of, say, adding a cable.

The phase offset can be specified from - 360° to +360° .

Using the Phase Offset Function

  1. Press Channel Next/Channel Prev and Trace Next/Trace prev to select the active phase trace which you want.

  2. Press Scale.

  3. Click Phase Offset, then enter the phase offset (° ) in the data entry area.

Velocity factor

The velocity factor is the ratio of the propagation velocity of a signal in a coaxial cable to the propagation velocity of that signal in free space. The velocity factor for a common cable is about 0.66. The propagation velocity depends on the dielectric constant (ƒÃr) of the dielectric substance the cable.

By specifying the velocity factor, you can match the equivalent length (in meters) appearing in the data entry area to the actual physical length when using the Electrical Delay or Setting port extensions to specify the electrical delay (in seconds).

You can define the velocity factor for each channel.

Using the velocity factor

  1.  Press Channel Next/Channel Prev to select the channel you want.

  2. Press Cal.

  3. Click Velocity Factor, then enter the velocity factor in the data entry area.

Port Extensions and Loss Values

Setting port extensions

Port Extension is a function for moving the calibration reference plane by specifying the electrical delay. This function is useful when you cannot directly perform calibration at the DUT terminal because the DUT is inside the test fixture. In such cases, this function enables you to first perform calibration at the test fixture terminal and then move the calibration plane to the DUT terminal by extending the port.

Port extension corrects the electrical delay of each test port (phase shift) only. It cannot remove errors caused by the loss in and incorrect matching of cables, adapters, or test fixtures.

Operational procedure

  1. Press Channel Next/Channel Prev to select the channel you want.

  2. Press Cal.

  3. Click Port Extensions > Extension Port 1/2.

  4. Specify Loss values by clicking Loss.

Setting coaxial delay, waveguide delay and cut off frequency

Follow the steps below to set coaxial or waveguide delays:

  1. Press Channel Next/Channel Prev to select the channel you want.

  2. Press Cal > Port Extensions

    Softkey

    Function

    Auto Port Extension

    Sets Auto Port Extension

    Extension Port 1

    Sets port extension (in seconds) for test port 1.

    Extension Port 2

    Sets port extension (in seconds) for test port 2.

  3. Click Extension Port n where n is 1 or 2.

  4. Click Waveguide to set delay in sec.

  5. Click Cutoff Frequency to set cut off frequency of selected port.

  6. Click Coax. Extension to set the coaxial extension in sec.

  7. If you want to use waveguide port extension, then it is not necessary to set coaxial delay. If only waveguide measurement is needed, coaxial delay should be set to zero. Coaxial extension value should be set while measuring adapters between coaxial and waveguide.

Waveguide delay and Cut off frequency can be set using the following commands:

SCPI.SENSe(Ch).CORRection.EXTension.PORT(Pt).WAVeguide.TIME

SCPI.SENSe(Ch).CORRection.EXTension.PORT(Pt).WAVeguide.CUToff

Setting loss values

In addition to port extension, you can set loss values for each port. By correcting loss due to port extension, more accurate measurement results are obtained.

There are two types of loss value settings: loss values at two frequency points for a specified port, and a DC loss value. You can make these settings at the same time for each port.

1. Setting loss values

  1. Press Channel Next/Channel Prev to select the channel you want.

  2. Press Cal > Port Extensions.

  3. Click Extension Port n where n is 1 or 2.

  4. Click Loss to set a loss value.

  5. Click Loss1 [OFF] to toggle to Loss1 [ON] (enabled), and enter a loss value (Loss1) and a frequency (Freq1).

  6. If you want to set loss at two frequency points, press Loss2 [OFF] to toggle to Loss [ON] (enabled), and enter a loss value (Loss2) and a frequency (Freq2).

  7. If you want to set loss values for other ports, repeat steps 3 to 6.

2. Setting a DC loss value

  1. Press Channel Next/Channel Prev to select the channel you want.

  2. Press Cal.

  3. Click Port Extensions > Loss.

  4. Click Select Port to select the port you want to set a DC loss value.

  5. Click Loss at DC, then enter a DC loss value.

  6.  If you want to set a DC loss value for other ports, repeat steps 4 and 5.

Enabling port extensions and loss values

  1. Press Channel Next/Channel Prev to select the channel you want.

  2. Press Cal > Port Extensions > Extensions > ON

Using the auto port extension function

The auto port extension function automatically measures port extension and loss values for each port using the OPEN/SHORT standard connection to the ports.

Softkey

Function

Auto Port Extension

Select Ports

Sets the Ports (1 or 2)

Measure OPEN

Performs a OPEN measurement

Measure SHORT

Performs a Short measurement

Method

Sets the Span

Include Loss

Sets Loss ON/OFF

Adjust Mismatch

Sets Adjust Mismatch ON/OFF

 

When the auto port extension function is completed, the port extensions and loss values are updated to the calculated values.

1. Selecting a port(s)

Select the port(s) for which you want to use the auto port extension function.

  1. Press Channel Next/Channel Prev to select the channel you want.

  2. Press Cal.

  3. Click Port Extensions > Auto Port Extension > Select Ports to select the corresponding port(s).

2. Setting frequencies used for calculation

Set the frequency points with which you want to calculate a loss value.

  1. Press Channel Next/Channel Prev to select the channel you want.

  2. Press Cal.

  3. Click Port Extensions > Auto Port Extension > Select Ports > Method to set the frequencies used for calculation.

     

    Softkey

    Function

    Current Span

    Executed using the frequency range set currently.

    Active Marker

    Executed using the frequency at the active marker. In this case, the result is applied to Loss1. Loss2 is ignored.

    User Span

    Executed using a start value and a stop value you set.

  1. If you have selected User Span, use User Span Start and User Span Stop to set a start value and a stop value.

  2. For Current Span and User Span, a frequency point at 1/4 of the frequency range is set to Freq1; a frequency point at 3/4 of the frequency range is set to Freq2.

  3. If the setting is not made before starting OPEN/SHORT standard measurement, it does not affect the calculation result.

3. Specifying a loss value as a calculation target

Specify whether you want to include a loss value in the calculation result.

  1. Press Channel Next/Channel Prev to select the channel you want.

  2. Press Cal.

  3. Click Port Extensions > Auto Port Extension > Select Ports > Include Loss to turn it on.

  4. If the setting is not made before starting the measurement of the OPEN/SHORT standard, it does not affect the calculation result.

4. Specifying a DC loss value as a calculation target

Specify whether you want to include a DC loss value in the calculation result.

  1. Press Channel Next/Channel Prev select the channel you want.

  2. Press Cal.

  3. Click Port Extensions > Auto Port Extension > Adjust Mismatch to turn it on.

  4. If the setting is not made before starting the measurement of the OPEN/SHORT standard, it does not affect the calculation result.

5. Measuring the OPEN/SHORT standard and executing calculation

Calculate port extensions and loss values based on the calculation results using the OPEN/SHORT standard.

  1. Press Channel Next/Channel Prev keys select the channel you want.

  2. Press Cal.

  3. Click Port Extensions > Auto Port Extension.

  4. If you use the OPEN standard, click Measure OPEN, and select the port(s) for which you want to execute measurement. Execution is restricted to ports selected in Selecting a port(s)

  5. If you use the SHORT standard, click Measure SHORT, and select the port(s) for which you want to execute measurement. Execution is restricted to ports selected in Selecting a port(s).

6. Deleting the result of open/short measurement

When you exit from the softkey menu in the same level after open/short measurement, the measurement results are deleted. Note that you can use a GPIB command.