Setting the Scales

Other topics about Setting Measurement Conditions

Auto Scale

The auto scale function is used to tailor each scale (scale/division and the reference line value) automatically in such a way that traces will appear at the proper size on the screen for easy observation.

Single Trace Auto Scale

Follow the procedure below to perform the auto scale function on a specific trace.

  1. Press Channel Next/Channel Prev and Trace Next/Trace Prev to select the trace for which the auto scale function will be performed.

  2. Press Scale > Auto Scale.

Auto Scale on All Traces Within a Channel

  1.  Press Channel Next/Channel Prev to select the channel for which the auto scale function will be performed.

  2.  Press Scale > Auto Scale.

Manual Scale Adjustment on a Rectangular Display Format

For a rectangular display format, four parameters are used to manually adjust the scales.

Adjustable feature

Description

Divisions

Defines the number of divisions on the Y-axis. An even number from 4 to 30 must be used. Once set, it is commonly applied to all traces displayed in any rectangular format within that channel.

Scale/Division (Scale/Div)

Defines the number of increments per division on the Y-axis. The value applies only to the active trace.

Reference position

Defines the position of the reference line. The position must be specified using the number assigned to each division on the Y-axis starting at 0 (the least significant) running up to the number of divisions being used (the most significant). The position applies only to the active trace.

Reference line value (Reference Value)

Defines the value corresponding to the reference line. It must be set using the unit on the Y-axis. The reference line value applies to the active trace only.

 

 

Setting the scales manually on a rectangular display format

  1. Press Channel Next/Channel Prev and Trace Next/Trace Prev to select the trace for which scale features will be adjusted.

  2.  Press Scale key.

  3. Select the softkey that corresponds to the particular feature that needs to be adjusted.
     

    Softkey

    Function

    Divisions

    Defines the number of divisions on the Y-axis.

    Scale/Div

    Defines the number of increments per division on the Y-axis.

    Reference Position

    Defines the position of the reference line.

    Reference Value

    Defines the value corresponding to the reference line.

Manual scale adjustment on the Smith chart/Polar format

Manual scale adjustment on the Smith chart format or the polar format is done by using the displacement (Scale/Div of the outermost circle).

 

Setting the scales manually on the Smith chart/polar format

  1. Press Channel Next/Channel Prev and Trace Next/Trace prev to select the trace for which the scale will be adjusted.

  2. Press Scale.

  3. Click Scale/Div, then input the displacement of the outermost circle.

Setting the value of a reference line using the marker

When using a rectangular display format, it is possible to change the reference line value to be equal to the response value of the active marker on the active trace.

Setting the reference line value using the marker

  1. Place the active marker on the active trace at the position that corresponds to the new reference line value.

  2. Press Scale or Marker Fctn.

  3. Click Marker -> Reference to change the reference line value to the marker response value.

  4. If the reference marker is turned ON and the stimulus value of the active marker is expressed using a value relative to the reference marker, the absolute stimulus value will be used to set the new reference line value.