Used to enter numeric data into the E5072A. Press a hardkey or softkey to enter data, and the data entry bar will appear at the top of the screen. To assign a title to a channel window, an entry bar that allows you to enter letters and symbols by using the front panel keys or mouse is displayed instead.
Data entry bar
To manipulate the data entry bar by using the front panel keys, the data entry bar must be selected as the object to manipulate (with the focus placed on it). When the focus is placed on the data entry bar, the entire bar is displayed in blue. Pressing or clicking Focus Key in the ENTRY Block enables you to move the focus to the desired object.
Closes the data entry area (turns off the display). Use mouse to manipulate this button.
When the data entry bar is displayed for the first time, the current settings are displayed on it. You can change numeric values by typing from the keyboard or in the ENTRY block on the front panel.
You can hide the frequency information in order to ensure its confidentiality or for other reasons. For detailed information, see Hiding Softkey's Frequency Information.
After entering numeric values in the data entry area by using the keyboard or the numeric keys in the ENTRY block on the front panel, press this button to finish the entry. Use the mouse to manipulate this button.
Displays the name of the parameter for which data will be entered.
Increases or decreases the numeric value in the data entry area in small steps. Use the mouse to manipulate this button.
Increases or decreases the numeric value in the data entry area in large steps. Use the mouse to manipulate this button.