Access jumpers on the E5072A allows for the E5072A to be configured. See System Description for the block diagram.
Ground terminal is provided with the E5072A and is connected to the chassis of the E5072A. You can connect a banana-type plug to this terminal for grounding.
A group of keys for selecting active channels and traces. For more on the concepts of channels and traces, see Setting Channels and Traces.
|
Key Name |
Description |
|
Channel Next |
Selects the next channel as the active channel. (Each time the key is pressed, the active channel steps one up to the next channel). A channel must be active before you can define parameters such as the sweep range. To change the settings of a channel, use this key to first make the channel active. |
|
Channel Prev |
Selects the previous channel as the active channel. (Each time the key is pressed, the active channel steps one down to the previous channel.) |
|
Trace Next |
Selects the next trace as the active trace. (Each time the key is pressed, the active trace steps one up to the next trace). A trace must be active before you can define measurement parameters and other settings. To change the settings of a trace, use this key to first make the trace active. |
|
Trace Prev |
Selects the previous trace as the active trace. (Each time the key is pressed, the active trace steps one down to the previous trace.) |
A group of keys used for entering numeric data is provided on the front panel of the E5072A.
|
Key Name |
Description |
|
0, 1, 2, 3 ..... 9 , . (numeric keys) |
Type numeric characters or a decimal point at the position of the cursor in the data entry area. |
|
+/- |
+/- alternately changes the sign (+, - ) of a numeric value in the data entry area. |
|
G/n, M/u, k/m, x1 |
Adds a prefix to the numeric data typed by using the numeric key and +/- key. One of the two prefixes written on the surface of the key is automatically selected depending on the parameter to be entered. x1 is entered without a prefix. |
|
Softkey On/Off , Entry Off |
Turns off the data entry bar if it is displayed. If the dialog box is displayed, cancels the entry and closes the dialog box. If the data entry bar and dialog box are not displayed, it turns the softkey menu display on/off. |
|
Bk Sp |
Backspace key. |
|
Focus |
Changes the selection (focus) among the objects to be manipulated by the NAVIGATION Block keys and ENTRY Block keys. The objects to be manipulated by the NAVIGATION Block keys and ENTRY Block keys include softkey menus, data entry areas, tables (e.g., segment tables, limit tables, and marker tables), and dialog boxes. When two or more of these are displayed on the screen and need selecting, use this key to change the selection (focus) among the objects to be manipulated. When a softkey menu is selected, the menu name area at the top of the menu is displayed in blue. When a data entry area is selected, the data entry bar is displayed in blue. When a table is selected, the frame of the table window is displayed in light gray. While a dialog box is displayed, the focus is fixed on the dialog box and cannot be changed. |
|
Help |
Displays help for E5072A. |
A group of keys related to the macro function, store and call function, control/management function, and presetting of the E5072A (returning it to the preset state).
|
Key Name |
Description |
|
Macro Setup |
Displays the Macro Setup Menu in Softkey Menu Bar. Manipulating the Macro Setup Menu enables you to start up the VBA editor or to create, call, or store a VBA project. |
|
Macro Run |
Executes a VBA procedure called "main" that has a VBA module named Module1. |
|
Macro Break |
Stops the VBA procedure being executed. |
|
Save/Recall |
Displays the Save/Recall Menu in Softkey Menu Bar. Manipulating the Save/Recall Menu enables you to store the setup conditions to or read from the storage devices, calibration data, and trace data of the analyzer. |
|
Capture/System |
First, temporarily saves the data for the image displayed on the LCD screen the moment this key is pressed to the internal memory (clipboard). Immediately after that, displays the System Menu in the Softkey Menu Bar. Manipulating the System Menu enables you to define the setup for the limit test and then execute it or to define the setup for the control and management of the analyzer. Using the Dump Screen Image option enables you to store the image data in the clipboard to a file on the storage devices. Also, using the Print option in the System Menu enables you to print the image data in the clipboard to a printer. |
|
Preset |
Displays the Preset Menu in Softkey Menu Bar. Clicking OK in the Preset Menu enables you to return the analyzer to the initial setup state, called the preset setup. |
A group of keys used for analyzing the measurement results by using the markers, fixture simulator and etc.
|
Key Name |
Description |
|
Marker |
Displays the Marker Menu in Softkey Menu Bar. Manipulating the Marker Menu enables you to turn the markers on/off and move them by entering stimulus values. You can place up to 10 markers on each trace. |
|
Marker Search |
Displays the Marker Search Menu in Softkey Menu Bar. Manipulating the Marker Search Menu enables you to move a marker to a specific point (maximum, minimum, peak, and a point with a target value) on a trace. You can also find the bandwidth parameters (up to six) and display them. |
|
Marker Fctn |
Displays the Marker Function Menu in Softkey Menu Bar. Manipulating the Marker Function Menu enables you to not only specify the marker sweep range and the coupling of markers on a channel but also to display statistics data on traces. |
|
Analysis |
Displays the Analysis Menu in Softkey Menu Bar. Manipulating the Analysis Menu enables you to use the analytical function. |
The keys and knob in the NAVIGATION Block are used to navigate between softkey menus, tables (limit table, segment table, etc.), or selected (highlighted) areas in a dialog box as well as to change a numeric value in the data entry area by stepping up or down. When selecting one of two or more objects (softkey menus, data entry areas, etc.) to manipulate with the NAVIGATION Block keys displayed on the screen, first press the Focus key in the ENTRY Block to select the object to be manipulated (placing focus on the object) and then manipulate the NAVIGATION Block keys (knob) to move among selected (highlighted) objects or change numeric values.
The following descriptions show how the NAVIGATION Block keys work both when the focus is on a softkey menu and when the focus is on the data entry area. For more on manipulating tables and dialog boxes, refer to the manipulation procedure for each of these functions.
When the focus is placed on a softkey menu (the menu title area in the uppermost part is displayed in blue), the NAVIGATION Block keys work as described below.
|
Key Name |
Description |
|
|
Moves the softkey selection (highlighted display) up or down. |
|
|
Moves the softkey selection (highlighted display) up or down. |
|
|
Displays the softkey menu one layer above. |
|
|
Displays the softkey menu one layer below. |
|
Enter or |
Executes the function of the selected softkey. |
After pressing the data entry softkey, the focus automatically moves to the data entry area.
When the focus is placed on the data entry area (the data entry bar is displayed in blue), the NAVIGATION Block keys work as described below.
|
Key Name |
Description |
|
|
Increases or decreases the numeric value in the data entry area in small steps. |
|
|
Increases or decreases the numeric value in the data entry area in large steps. |
|
|
Moves the cursor (|) in the data entry area laterally back and forth. Use it together with the ENTRY Block keys to change data one character at a time. |
|
Enter or |
Finishes the entry in the data entry area and moves the focus to the softkey menu. |
A group of keys used mainly for setting up response measurements on the E5072A.
|
Key Name |
Description |
|
Channel Max |
Changes between normal and maximum display of the active channel window. In normal display, all defined channel windows (both active and non-active) are displayed in split views on the screen. In maximum display, only the active channel window is displayed over the entire area, while non-active windows are not displayed. To maximize the active channel, double-click the channel window frame. Measurements are also carried out on non-active channels that are not displayed. |
|
Trace Max |
Changes between normal and maximum display of the active trace window. In normal display, all defined trace windows (both active and non-active) are displayed in split views on the screen. In maximum display, only the active trace is displayed over the entire channel window, while non-active traces are not displayed. To maximize the trace, double-click anywhere in the channel window. Measurements are also carried out on non-active traces that are not displayed. |
|
Meas
|
Displays the Measurement Menu in Softkey Menu Bar. Manipulating the Measurement Menu enables you to specify the measurement parameters (types of S-parameters) for each trace. |
|
Format |
Displays the Format Menu in Softkey Menu Bar. Manipulating the Format Menu enables you to specify the data format (data transformation and graph formats) for each trace. |
|
Scale |
Displays the Scale Menu in Softkey Menu Bar. Manipulating the Scale Menu enables you to specify the scale for displaying a trace (magnitude per division, value of the reference line, etc.) for each trace. You can also specify the electrical delay and phase offset for each trace. |
|
Display |
Displays the Display Menu in Softkey Menu Bar. Manipulating the Display Menu enables you to specify the number of channels and the channel window array, the number and arrangement of traces, the setup for data math, etc. |
|
Avg |
Displays the Average Menu in Softkey Menu Bar. Manipulating the Average Menu enables you to define the averaging, smoothing, and IF bandwidth. |
|
Cal |
Displays the Calibration Menu in Softkey Menu Bar. Manipulating the Calibration Menu enables you to turn the calibration and error correction on/off and change definitions for calibration kits. |
A group of keys for defining the stimulus values (signal sources and triggers).
|
Key Name |
Description |
|
Start |
Displays the data entry bar for specifying the start value of the sweep range in the upper part of the screen. (It also displays the Stimulus Menu for specifying the sweep range in Softkey Menu Bar.) |
|
Stop |
Displays the data entry bar for specifying the stop value of the sweep range in the upper part of the screen. (It also displays the Stimulus Menu in the same way as Start.) |
|
Center |
Displays the data entry bar for specifying the center value of the sweep range in the upper part of the screen. (It also displays the Stimulus Menu in the same way as Start.) |
|
Span |
Displays the data entry bar for specifying the span value of the sweep range in the upper part of the screen. (It also displays the Stimulus Menu in the same way as Start.) |
|
Sweep Setup |
Displays the Sweep Setup Menu in Softkey Menu Bar. Manipulating the Sweep Setup Menu enables you to specify the signal source power level, sweep time, number of points, sweep type, etc. |
|
Trigger |
Displays the Trigger Menu in Softkey Menu Bar. Manipulating the Trigger Menu enables you to specify the trigger mode and trigger source. You can specify the trigger mode for each channel. |
The E5072A is equipped with a 10.4-inch TFT color, touch-sensitive LCD screen for displaying traces, scales, settings, softkeys and other measurement related information. The touch screen LCD allows you to manipulate softkeys by touching the LCD screen directly with a finger. For more on the LCD screen, see Screen Area: Names and Functions of Parts.
Do not press the surface of the LCD screen with a sharp object (e.g., a nail, pen, or screwdriver). Pressing the surface with a sharp-pointed object will damage the LCD screen surface or cause the screen to fail.
Valid pixels are 99.998 % and more. Below 0.002 % of fixed points of black, blue, green or red are not regarded as failure.
The E5072A comes with two ports that can be used to provide power to external probes. See the Data sheet for the voltage and maximum current.
This switch can turn on/off the E5072A. The color on the button shows the status as shown below:
|
Indicator Color |
Description |
|
Green |
Normal power on status. |
|
Orange |
Standby status. |
|
Red |
To turn off the power for the E5072A, be sure to follow the steps described below:
First, press this standby switch or send a shutdown command from the external controller to activate the shutdown process (the processing of software and hardware necessary to turn off the power supply). This will put the E5072A into the standby state.
Next, if necessary, turn off power supply to the Power Cable Receptacle (to LINE) on the rear panel.
Under normal use, never directly interrupt the power supply to the power cable receptacle on the rear panel when the power supply is on. Always keep the Line Switch (Always ON) at (|). Never turn it off (O).
If you directly interrupt the power supply to the power cable receptacle when the power supply is on, or turn off the Line Switch (Always ON), the shutdown process will not work. This could damage the software and hardware of the E5072A and lead to device failure.
Turning on the power supply after a faulty shutdown may cause the system to start up in a condition called "safe mode." If this occurs, first shut down the system to put it into the standby state and then turn on the power supply again to start up the system in normal mode.
The port to which the DUT is connected. While signals are being output from a test port, the yellow LED above the test port is lit.
Do not apply DC voltage or current to the test port. Applying DC voltage or current may lead to device failure. In particular, the capacitor might remain charged. Connect the measurement sample (DUT) to the test port (or the test fixture, cables, etc. connected to the test port) after the analyzer has been completely discharged. The maximum DC limit of test port is 35V.
The test ports comply with Installation Category I of IEC 61010-1.
Two USB (Universal Serial Bus) ports are provided that can be used for connecting to ECal (Electronic Calibration) module, USB, Multiport test set or a printer. Connecting a designated ECal module to this port enables ECal measurements to be obtained. Connecting a compatible printer to this port enables screen information on the E5072A to be printed. For more on executing ECal measurements, see Calibration, and for printing, see Printing Displayed Screen. See Using USB for more details.