Other topics about Maintenance
Users can update E5072A firmware by themselves. Updating firmware does not include the following software update:
Windows Operating System
VBA (Visual Basic for Application)
Driver for Windows
Calibration Constant Data
Press System > Service Menu > Exit to terminate the E5072A application.
Download the latest firmware from the download site. (E5072.exe). f you use your local PC to download, save the file to a USB mass storage device in order to move it to E5072A, then connect the USB mass storage device into the front USB port of the E5072A.
Double click E5072.exe to install the firmware.
Follow the instruction of windows installer. After the installation is finished, the instrument restarts.
Press System > Firmware Revision to confirm the firmware revision you have just installed.
Visit http://www.keysight.com/find/ena_support, then click Firmware Download for E5072A.
Download the latest firmware file.
Download the execution file (E5072A_xx.xx.exe).
Run the E5072A_xx.xx.exe to extract the E5072A.msi.
If you use your local PC to download, save the file to a USB mass storage device in order to move it to E5072A. Connect the USB mass storage device into the front USB port of the E5072A.
Copy or move the E5072A.msi file to D drive.
Press System > Service Menu > Update Firmware. Then, the password dialog box appears.
Type e507xa as the password, then click OK.
In Open dialog box, select E5072A.msi, then press Open. Then the windows installer appears.
Follow the instruction of windows installer.
After the installation is finished, the firmware restarts.
Press System > Firmware Revision to confirm the firmware revision you have just installed.