Code Migration Tools

This section provides useful information to migrate the automation system from 8753 to ENA.

Other topics about Replacing 8753ES with E5072A

Code Conversion Assistant Editor

The code conversion assistant editor helps to convert 8753 GPIB commands to ENA commands. This software consists of a text editor (EmEditor) and a plug-in software, which works on a PC and helps to edit programs in text format. The editor is also useful for 872X analyzers as most of the 872X commands are the same as 8753’s. The software can be downloaded from www.keysight.com/find/ena_support.

ENA 8753 Code Translator (E5072_8753cXL) Application

The E5072_8753cXL is a code emulation application that allows you to use the ENA with the test program that was written in language for 8753 series network analyzer. This application works on background of the ENA, translating incoming 8753 commands via GPIB in real time.

The installer is pre-loaded on the E5072A hard disk drive  (D:\Agilent\ENACXL\Keysight_E5072_8753cXL.msi).

To install the E5072_8753cXL application, follow the instruction below.

1. Terminate the ENA application: Press System > Service Menu > Exit.

2. Double-click the Keysight_E5072_8753cXL.msi to launch the installer.

3. Follow the wizard to install the E5072_8753cXL.

After the installation is complete, the following files will be available from the Windows start menu. Refer to the “Help Manual” for more details on launching and using the E5072_8753cXL.