Method (Write-only)
Prompt(Mes)
Displays the message you specify on the instrument status bar (at the bottom of the LCD display) and suspends the program until the Macro Setup > Continue button is pressed. (No read)
When using this object, execute the program with the Visual Basic closed since you need to press the Macro Setup > Continue. For more information, see Running a Program from the E5072A Measurement Screen. If you need to abort the program, see Stopping with the Dialog Box Appeared.
Parameter |
Mes |
Description |
Message |
Data type |
Character string type (String) |
Prompt ("Connect DUT, and then press [Continue]")
No equivalent key is available on the front panel.