SCPI.CALCulate(Ch).SELected.MATH.EMEMorize

Object type

Method (Write-only)

Syntax

SCPI.CALCulate(Ch).SELected.MATH.EMEMorize

 

The following syntax is also supported:

SCPI.CALCulate(Ch).TRACe(Tr).MATH.EMEMorize

Description

This command copies the calculated equation data to the memory trace for the active trace of selected channel (Ch).

 

Optionally, you can select the trace and copy the calculated equation data to the memory trace, for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.

Examples

SCPI.CALCulate(1).SELected.MATH.EMEMorize

Related objects

SCPI.CALCulate(Ch).PARameter(Tr).SELect

SCPI.CALCulate(Ch).SELected.MATH.MEMorize

Equivalent key

Display > Equation > Mem

Equivalent SCPI command

Syntax

:CALCulate{[1]-160}[:SELected]:MATH:EMEMorize

 

 The following syntax is also supported:

:CALCulate{[1]-160}:TRACe{[1]-16}:MATH:EMEMorize

Example of use

10 OUTPUT 717;":CALC1:MATH:EMEM"