Method (Write-only)
SCPI.CALCulate(Ch).SELected.MATH.MEMorize
The following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).MATH.MEMorize
This command copies the measurement data to the memory trace, for the active trace of selected channel (Ch).
Optionally, you can select the trace and copy the measurement data to the memory trace, for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.MATH.MEMorize
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.MATH.EMEMorize
Display > Data - > Mem
:CALCulate{[1]-160}[:SELected]:MATH:MEMorize
The following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:MATH:MEMorize
10 OUTPUT 717;":CALC1:MATH:MEM"