Property (Read-Write)
SCPI.CALCulate(Ch).FSIMulator.BALun.TOPology.BALanced.PPORts = Ports
Ports = SCPI.CALCulate(Ch).FSIMulator.BALun.TOPology.BALanced.PPORts
This command assigns each port when the balance device type is "balance", for the selected channel (Ch).
To set the balance device type to "balance," specify BAL with the SCPI.CALCulate(Ch).FSIMulator.BALun.DEVice object.
Parameter |
Ports |
Description |
Indicates 2-element array data (port number).
The index of the array starts from 0. |
Data type |
Variant type (Variant) |
Range |
1 to 2 |
Preset value |
Ports(0):1 / Ports(1):2 |
Resolution |
1 |
Note |
If the specified variable is out of the allowable setup range, an error occurs when executed. If you specify the same port number to 2 or more port numbers, an error occurs when executed. |
Dim BbalPort As Variant
SCPI.CALCulate(1).FSIMulator.BALun.DEVice = "bal"
SCPI.CALCulate(1).FSIMulator.BALun.TOPology.BALanced.PPORts = Array(1,4)
BbalPort = SCPI.CALCulate(1).FSIMulator.BALun.TOPology.BALanced.PPORts
Dim BbalPort(1) As Variant
Dim Ref As Variant
BbalPort(0) = 1
BbalPort(1) = 4
SCPI.CALCulate(1).FSIMulator.BALun.DEVice = "bbal"
SCPI.CALCulate(1).FSIMulator.BALun.TOPology.BALanced.PPORts = BbalPort
Ref = SCPI.CALCulate(1).FSIMulator.BALun.TOPology.BALanced.PPORts
SCPI.CALCulate(Ch).FSIMulator.BALun.DEVice
Analysis > Fixture Simulator > Topology > Port1(bal)
When performing the operation from the front panel, set each port separately.
:CALCulate{[1]-160}:FSIMulator:BALun:TOPology:BALanced
[:PPORts] <numeric 1>, <numeric 2>
:CALCulate{[1]-160}:FSIMulator:BALun:TOPology:BALanced
[:PPORts]?
{numeric 1},{numeric 2}<newline><^END>
10 OUTPUT 717;":CALC1:FSIM:BAL:TOP:BAL 1,4"
20 OUTPUT 717;":CALC1:FSIM:BAL:TOP:BAL?"
30 ENTER 717;A,B