Property (Read Only)
Value = SCPI.CALCulate(Ch).SELected.FUNCtion.POINts
The following syntax is also supported:
Value = SCPI.CALCulate(Ch).TRACe(Tr).FUNCtion.POINts
This command reads the number of data pairs of the analysis result of the SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute object, for the active trace of selected channel (Ch).
For the analysis of the mean value or the search of the maximum value, 1 is always read out; for the search of all peaks or the search of all targets, the total number of searched measurement points is read out.
Optionally, you can select the trace and read the number of data pairs of the analysis result of the SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute object for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Value |
|
Description |
Number of analyzed data pairs |
|
Data type |
Long integer type (Long) |
|
Preset Value |
0 |
Dim AnaPoin As Long
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.FUNCtion.TYPE = "ape"
SCPI.CALCulate(1).SELected.FUNCtion.EXECute
AnaPoin = SCPI.CALCulate(1).SELected.FUNCtion.POINts
SCPI.CALCulate(Ch).SELected.FUNCtion.DATA
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute
No equivalent key is available on the front panel.
:CALCulate{[1]-160}[:SELected]:FUNCtion:POINts?
The following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:FUNCTion:POINts?
{numeric}<newline><^END>
10 OUTPUT 717;":CALC1:FUNC:POIN?"
20 ENTER 717;A