Property (Read-Write)
SCPI.CALCulate(Ch).SELected.FUNCtion.TARGet = Value
Value = SCPI.CALCulate(Ch).SELected.FUNCtion.TARGet
The following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).FUNCtion.TARGet = Value
Value = SCPI.CALCulate(Ch).TRACe(Tr).FUNCtion.TARGet
This command sets/gets the target value when performing the target search with the SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute object, for the active trace of the selected channel (Ch).
Optionally, you can select the trace and set/get the target value when performing the target search with the SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute object for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Value |
|
Description |
Target value |
|
Data type |
Double precision floating point type (Double) |
|
Range |
-5E8 to 5E8 |
|
Preset value |
0 |
|
Unit |
Varies depending on the data format.
|
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
Dim TargVal As Double
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.FUNCtion.TYPE = "atar"
SCPI.CALCulate(1).SELected.FUNCtion.TARGet = -12.5
TargVal = SCPI.CALCulate(1).SELected.FUNCtion.TARGet
SCPI.CALCulate(Ch).SELected.FUNCtion.DATA
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.FUNCtion.TYPE
SCPI.CALCulate(Ch).SELected.FUNCtion.TTRansition
SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute
No equivalent key is available on the front panel.
:CALCulate{[1]-160}[:SELected]:FUNCtion:TARGet <numeric>
:CALCulate{[1]-160}[:SELected]:FUNCtion:TARGet?
The following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:FUNCtion:TARGet <numeric>
:CALCulate{[1]-160}:TRACe{[1]-16}:FUNCtion:TARGet?
{numeric}<newline><^END>
10 OUTPUT 717;":CALC1:FUNC:TARG -12.5"
20 OUTPUT 717;":CALC1:FUNC:TARG?"
30 ENTER 717;A