Property (Read-Write)
SCPI.CALCulate(Ch).SELected.RLIMit.STATe = Status
Status = SCPI.CALCulate(Ch).SELected.RLIMit.STATe
The following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).RLIMit.STATe = Status
Status = SCPI.CALCulate(Ch).TRACe(Tr).RLIMit.STATe
This command turns ON/OFF the ripple test function for the active trace (specified with the SCPI.CALCulate(Ch).PARameter(Tr).SELect command) of selected channel (Ch).
Optionally, you can select the trace and turn ON/OFF the ripple test function for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Status |
|
Description |
ON/OFF the ripple test function |
|
Data type |
Boolean type (Boolean) |
|
Range |
Select from the following:
|
|
Preset value |
False or OFF |
Dim RLimTest As Boolean
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.RLIMit.STATe = True
RLimTest = SCPI.CALCulate(1).SELected.RLIMit.STATe
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.RLIMit.DATA
SCPI.CALCulate(Ch).SELected.RLIMit.DISPlay.LINE
SCPI.CALCulate(Ch).SELected.RLIMit.DISPlay.SELect
SCPI.CALCulate(Ch).SELected.RLIMit.DISPlay.VALue
SCPI.CALCulate(Ch).SELected.RLIMit.FAIL
SCPI.CALCulate(Ch).SELected.RLIMit.REPort.DATA
Analysis > Ripple Limit > Ripple Limit Test
:CALCulate{[1]-160}[:SELected]:RLIMit[:STATe] {ON|OFF|1|0}
:CALCulate{[1]-160}[:SELected]:RLIMit[:STATe]?
The following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:RLIMit[:STATe] {ON|OFF|1|0}
:CALCulate{[1]-160}:TRACe{[1]-16}:RLIMit[:STATe]?
{1|0}<newline><^END>
10 OUTPUT 717;":CALC1:RLIM ON"
20 OUTPUT 717;":CALC1:RLIM?"
30 ENTER 717;A