Property (Read-Write)
SCPI.CALCulate(Ch).SELected.RLIMit.DATA = Data
Data = SCPI.CALCulate(Ch).SELected.RLIMit.DATA
The following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).RLIMit.DATA = Data
Data = SCPI.CALCulate(Ch).TRACe(Tr).RLIMit.DATA
This command sets/gets the ripple limit table for the active trace (specified with the SCPI.CALCulate(Ch).PARameter(Tr).SELect command)of selected channel (Ch).
The data transfer format when this command is executed depends on the setting with the SCPI.FORMat.DATA command.
Optionally, you can select the trace and set/get the ripple limit table for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Status |
|
Description |
Indicates the array data (for ripple line) of 1 + Num (number of limit lines)\ 4. Where n is an integer between 1 and Num.
The index of the array starts from 0. |
|
Data type |
Variant type (Variant) |
|
Note |
If there is no array data of 1+Num (number of set lines))*4 when setting a formatted memory array, an error occurs when executed and the object is ignored. For Data(n \ 4-3) in the array data, if you specify an integer other than 0 or 1, an error occurs when executed. For Data(n* 4-2) and Data(n * 4-1) in the array data, if the specified value is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
Dim RLimData As Variant
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.RLIMit.DATA = Array(1,1,1E6,1E9,0)
RLimData = SCPI.CALCulate(1).SELected.RLIMit.DATA
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.RLIMit.DATA = Array(0) ''' Clear Ripple Limit Table
Dim RlimData(5) As Variant
Dim Ref As Variant
RLimData(0) = 1
RLimData(1) = 1
RLimData(2) = 1e6
RLimData(3) = 1e9
RLimData(4) = 0
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.RLIMit.DATA = RLimData
Ref = SCPI.CALCulate(1).SELected.RLIMit.DATA
Dim RLimData(0) as Variant
RLimData(0) = 0
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.RLIMit.DATA = RLimData ''' Clear Ripple Limit Table
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.RLIMit.STATe
Analysis > Ripple Limit > Edit Ripple Limit > Add
:CALCulate{[1]-160}[:SELected]:RLIMit:DATA <numeric 1>,… ,<numeric 1+(N\ 4)>
:CALCulate{[1]-160}[:SELected]:RLIMit:DATA?
The following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:RLIMit:DATA <numeric 1>,… ,<numeric 1+(N\ 4)>
:CALCulate{[1]-160}:TRACe{[1]-16}:RLIMit:DATA?
{numeric 1},… ,{numeric 1+(Nx4)}<newline><^END>
10 DIM B(1:2,1:4)
20 OUTPUT 717;":CALC1:RLIM:DATA 2,1,1E9,3E9,3,1,5E9,7E9,3"
30 OUTPUT 717;":CALC1:RLIM:DATA?"
40 ENTER 717;A,B(*)
10 OUTPUT 717;":CALC1:RLIM:DATA 0" ! Clear Ripple Limit Table