Property (Read-Write)
SCPI.FORMat.BORDer = Param
Param = SCPI.FORMat.BORDer
This command sets/gets the transfer order of each byte in the output data (byte order), when the data transfer format is set to binary mode (by specifying "REAL" with SCPI.FORMat.DATA object).
This object is NOT used when controlling the E5072A using COM objects through E5072A VBA.
|
Parameter |
Param |
|
Description |
Byte order |
|
Data type |
Character string type (String) |
|
Range |
Select from the following: "NORMal": Specifies the byte order in which transfer starts from the byte including MSB (Most Significant Bit). "SWAPped": Specifies the byte order in which transfer starts from the byte including LSB (Least Significant Bit). |
|
Preset value |
"NORMal" |
Dim BitOrd As String
SCPI.FORMat.BORDer "swap"
BitOrd = SCPI.FORMat.BORDer
No equivalent key is available on the front panel.
:FORMat:BORDer {NORMal|SWAPped}
:FORMat:BORDer?
{NORM|SWAP}<newline><^END>
10 OUTPUT 717;":FORM:BORD SWAP"
20 OUTPUT 717;":FORM:BORD?"
30 ENTER 717;A$