Property (Read-Write)
SCPI.FORMat.DATA = Param
Param = SCPI.FORMat.DATA
This command can be used to set/get format data using the following SCPI commands:
:CALC{1-160}:DATA:FDAT
:CALC{1-160}:DATA:FMEM
:CALC{1-160}:DATA:SDAT?
:CALC{1-160}:DATA:SMEM?
:CALC{1-160}:FUNC:DATA?
:CALC{1-160}:LIM:DATA
:CALC{1-160}:LIM:REP?
:CALC{1-160}:LIM:REP:ALL?
:CALC{1-160}:BLIM:REP?
:CALC{1-160}:RLIM:DATA?
:CALC{1-160}:RLIM:REP?
:SENS{1-160}:CORR:COEF
:SENS{1-160}:FREQ:DATA?
:SENS{1-160}:SEGM:DATA
:SOUR:POW:PORT:CORR:COLL:TABL:ASEN:DATA
:SOUR:POW:PORT:CORR:COLL:TABL:BSEN:DATA
:SOUR{1-160}:POW:PORT{1-2}:CORR:COLL:TABL:LOSS:DATA
:SOUR{1-160}:POW:PORT{1-2}:CORR:DATA
ASCII transfer format must be specified when controlling the E5072A using SCPI commands with the Parse object in the E5072A VBA.
|
Parameter |
Param |
|
Description |
Data transfer format |
|
Data type |
Character string type (String) |
|
Range |
Select from the following: "ASCii": Specifies the ASCII transfer format. "REAL": Specifies the IEEE 64-bit floating point binary transfer format. "REAL32": Specifies the IEEE 32-bit floating point binary transfer format. |
|
Preset value |
"ASCii" |
Dim Fmt As String
SCPI.FORMat.DATA = "ASC"
Fmt = SCPI.FORMat.DATA
No equivalent key is available on the front panel.
:FORMat:DATA {ASCii|REAL|REAL32}
:FORMat:DATA?
{ASC|REAL|REAL32}<newline><^END>
10 OUTPUT 717;":FORM:DATA REAL"
20 OUTPUT 717;":FORM:DATA?"
30 ENTER 717;A$