Property (Read-Write)
SCPI.INITiate(Ch).CONTinuous = Status
Status = SCPI.INITiate(Ch).CONTinuous
This command turns ON/OFF the continuous initiation mode (where the trigger system initiates continuously) for the selected channel (Ch) in the trigger system. For more information, see Trigger System.
|
Parameter |
Status |
|
Description |
ON/OFF of the continuous initiation mode |
|
Data type |
Boolean type (Boolean) |
|
Range |
Select from the following:
|
|
Preset value |
Varies depending on [variable (Ch)] |
Dim ContMode As Boolean
SCPI.INITiate(2).CONTinuous = True
ContMode = SCPI.INITiate(2).CONTinuous
Trigger > Continuous (continuous initiation mode ON)
Trigger > Hold (continuous initiation mode OFF)
:INITiate{[1]-160}:CONTinuous {ON|OFF|1|0}
:INITiate{[1]-160}:CONTinuous?
{1|0}<newline><^END>
10 OUTPUT 717;":INIT1:CONT OFF"
20 OUTPUT 717;":INIT1:CONT?"
30 ENTER 717;A