Method (Write-only)
SCPI.INITiate(Ch).IMMediate
This command changes the state of each selected channel (Ch) to the initiation state in the trigger system.
When this object is executed for a channel in the idle state in the trigger system, it goes into the initiation state immediately. Then, after measurement is executed once, it goes back to the idle state.
If this object is executed for a channel that is not in the idle state or a channel for which the continuous initiation mode is set to ON (setting by which the trigger system initiates continuously) in the trigger system, an error occurs when executed and the object is ignored. For more information on the trigger system, see Trigger System.
SCPI.INITiate(1).CONTinuous = False
SCPI.INITiate(1).IMMediate
Trigger > Single
:INITiate{[1]-160}[:IMMediate]
10 OUTPUT 717;":INIT1"