Method (Write-only)
SCPI.SENSe(Ch).CORRection.COLLect.ACQuire.OLOad.LOAD.EXECute = Port
This command measures the calibration data of an offset load standard for the specified port, for the selected channel (Ch).
Parameter |
Port |
Description |
Port number |
Data type |
Long integer type (Long) |
Range |
1 to 2 |
Note |
If the specified variable is out of the allowable setup range, an error occurs when executed. |
Dim Dmy As Long
' Select X11644 Calibration Kit
SCPI.SENSe.CORRection.COLLect.CKIT.SELect = 15
' Select Load 2 in Load
SCPI.SENSe.CORRection.COLLect.ACQuire.SUBClass = 2
' Select Offset Line 1 (Thur). The "Thru" is defined as the standard No. 6 in the Define Standard.
SCPI.SENSe.CORRection.COLLect.ACQuire.OLOad.LINE = 6
MsgBox "Connect Offset Load (Thru)"
' Make a measurement for Offset Line 1
SCPI.SENSe.CORRection.COLLect.ACQuire.OLOad.Load.EXECute = 1
' Wait for measurement end.
Dmy = SCPI.IEEE4882.OPC
' Select Offset Line 2 (X-Band Delay Line).The "X-Band Delay Line" is defined as the standard No. 7 in the Define Standard.
SCPI.SENSe.CORRection.COLLect.ACQuire.OLOad.LINE = 7
MsgBox "Connect Offset Load (X-Band Delay Line)"
' Make a measurement for Offset Line 2
SCPI.SENSe.CORRection.COLLect.ACQuire.OLOad.Load.EXECute = 1
' Wait for measurement end.
Dmy = SCPI.IEEE4882.OPC
' Finalize the Offset load measurement.
SCPI.SENSe.CORRection.COLLect.ACQuire.OLOad.Load.DONE = 1
SCPI.SENSe(Ch).CORRection.COLLect.ACQuire.OLOAD.LINE
SCPI.SENSe(Ch).CORRection.COLLect.ACQuire.OLOAd.LOAD.DONE
SCPI.SENSe(Ch).CORRection.COLLect.ACQuire.OLOad.LOAD.COUNt
SCPI.SENSe(Ch).CORRection.COLLect.ACQuire.OLOad.LOAD.CLEar
Cal > Calibrate > Enhanced Response > Load > Load n - Offset Load> Offset Line n
Cal > Calibrate > 1-Port Cal > Load > Load n - Offset Load > Offset Line n
Cal > Calibrate > 2-Port Cal > Reflection > Port 1 Load > Load2 - Offset Load > Offset Line 2
:SENSe{[1]-160}:CORRection:COLLect[:ACQuire]:OLOad:LOAD[:EXECute] <numeric>
10 OUTPUT 717;":SENS1:CORR:COLL:OLO:LOAD 1"
20 OUTPUT 717;"*OPC?"
30 ENTER 717;A
Refer to Example for COM.