SCPI.SENSe(Ch).FREQuency.STOP

Object type

Property (Read-Write)

Syntax

SCPI.SENSe(Ch).FREQuency.STOP = Value

Value = SCPI.SENSe(Ch).FREQuency.STOP

Description

This command sets/gets the stop value of the sweep range of selected channel (Ch).

Variable

Parameter

Value

Description

Stop value

Data type

Double precision floating point type (Double)

Range

See frequency range for each option

Preset value

Maximum frequency in the range

Unit

Hz (hertz)

Resolution

1

Note

If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is breached) or the maximum value (if the upper limit of the range is exceeded) is set.

Examples

Dim Stp As Double
SCPI.SENSe(1).FREQuency.STOP = 3E9
Stp = SCPI.SENSe(1).FREQuency.STOP

Related objects

SCPI.SENSe(Ch).FREQuency.STARt

Equivalent key

Stop

Equivalent SCPI command

Syntax

:SENSe{[1]-160}:FREQuency:STOP <numeric>

:SENSe{[1]-160}:FREQuency:STOP?

Query response

{numeric}<newline><^END>

Example of use

10 OUTPUT 717;":SENS1:FREQ:STOP 100E6"
20 OUTPUT 717;":SENS1:FREQ:STOP?"
30 ENTER 717;A