Property (Read-Write)
SCPI.SOURce(Ch).POWer.PORT(Pt).ALC.MODE.RECeiver.IFBW = Value
Value= SCPI.SOURce(Ch).POWer.PORT(Pt).ALC.MODE.RECeiver.IFBW
This command sets/gets the fast IFBW of the receiver leveling sweep for the selected channel (Ch) and port (Pt).
|
Parameter |
Value |
|
Description |
Sets/gets the fast IFBW of the leveling sweep |
|
Data type |
Double precision floating point type (Double) |
|
Range |
10 to 500000 |
|
Preset value |
70000 |
Dim varIFBW As Double
varIFBW = 100
SCPI.SOURce(1).POWer.PORT(1).ALC.MODE.RECeiver.IFBW = varIFBW
varIFBW = SCPI.SOURce(1).POWer.PORT(1).ALC.MODE.RECeiver.IFBW
SCPI.SOURce(Ch).POWer.PORT(Pt).ALC.MODE.RECeiver.FAST
SCPI.SOURce(Ch).POWer.PORT(Pt).ALC.MODE.RECeiver.STATe
Sweep Setup > Power > Receiver Leveling > Port 1|Port 2 > Fast IFBW
:SOURce{[1]-160}:POWer:PORT{[1]|2}:ALC:MODE:RECeiver:IFBW {value}
:SOURce{[1]-160}:POWer:PORT{[1]|2}:ALC:MODE:RECeiver:IFBW?
<value><newline><^END>
10 OUTPUT 717;":SOUR1:POW:PORT1:ALC:MODE:REC:IFBW 0"
20 OUTPUT 717;":SOUR1:POW:PORT1:ALC:MODE:REC:IFBW?"
30 ENTER 717;A