Property (Read-Write)
SCPI.SOURce(Ch).POWer.PORT(Pt).ALC.MODE.RECeiver.STATe = Status
Status= SCPI.SOURce(Ch).POWer.PORT(Pt).ALC.MODE.RECeiver.STATe
This command turns ON/OFF the Receiver Leveling function for the selected channel (Ch) and port (Pt).
|
Parameter |
Status |
|
Description |
Turns ON/OFF the receiver leveling function |
|
Data type |
Boolean type (Boolean) |
|
Range |
Select from either of the following:
|
|
Preset value |
False or OFF |
Dim state As Boolean
SCPI.SOURce(1).POWer.PORT(1).ALC.MODE.RECeiver.STATe = True
state= SCPI.SOURce(1).POWer.PORT(1).ALC.MODE.RECeiver.STATe
SCPI.SOURce(Ch).POWer.PORT(Pt).ALC.MODE.RECeiver.IFBW
SCPI.SOURce(Ch).POWer.PORT(Pt).ALC.MODE.RECeiver.FAST
Sweep Setup > Power > Receiver Leveling > Port 1|Port 2 > Leveling
:SOURce{[1]-160}:POWer:PORT{[1]|2}:ALC:MODE:RECeiver[:STATe] {ON|OFF|1|0}
:SOURce{[1]-160}:POWer:PORT{[1]|2}:ALC:MODE:RECeiver[:STATe]?
{1|0}<newline><^END>
10 OUTPUT 717;":SOUR1:POW:PORT1:ALC:MODE:REC ON"
20 OUTPUT 717;":SOUR1:POW:PORT1:ALC:MODE:REC?"
30 ENTER 717;A