SCPI.SOURce(Ch).POWer.PORT(Pt).ATTenuation.DATA

Object type

Property (Read-Write)

Syntax

SCPI.SOURce(Ch).POWer.PORT(Pt).ATTenuation.DATA = Value

Value = SCPI.SOURce(Ch).POWer.PORT(Pt).ATTenuation.DATA

Description

This command sets/gets the power range for each port (Pt).

The power range is selected depending on the setting of the attenuator. The relationship between the attenuator value and the power range is available below:

Source Power Range

Step Attenuation

-49 ~ +20 dBm

0 dB

-59 ~ +10 dBm

10 dB

-69 ~  0 dBm

20 dB

-79 ~ -10 dBm

30 dB

-89 ~ -20 dBm

40 dB

-99 ~ -30 dBm

50 dB

-109 ~ -40 dBm

60 dB

 

Variable

Parameter

Value

Description

Dummy Parameter

Data type

Long integer type (Long)

Range

0 to 60

Preset value

0

Unit

dB

Resolution

10

Examples

Dim Att As Long
SCPI.SOURce(1).POWer.PORT(1).ATTenuation.DATA = 10
Att = SCPI.SOURce(1).POWer.PORT(1).ATTenuation.DATA

Related objects

SCPI.SOURce(Ch).POWer.PORT.ATTenuation.COUPle

Equivalent key

Sweep Setup > Power > Port Pwr&Att > Port 1 Pwr&Att|Port 2 Pwr&Att > Source Atten. > 0 dB|10 dB|20 dB|30 dB|40 dB|50 dB|60 dB

Equivalent SCPI command

Syntax

:SOURce{[1]-160}:POWer:PORT{[1]|2}ATTenuation[:DATA] <numeric>

:SOURce{[1]-160}:POWer:PORT{[1]|2}ATTenuation[:DATA]?

Query response

<numeric><newline><^END>

Example of use

10 OUTPUT 717;":SOUR1:POW:PORT1:ATT 0"
20 OUTPUT 717;":SOUR1:POW:PORT1:ATT?"
30 ENTER 717;A