SCPI.STATus.QUEStionable.BLIMit.CHANnel(Ch).PTRansition

Object type    

Property (Read-Write)

Syntax         

SCPI.STATus.QUEStionable.BLIMit.CHANnel(Ch).PTRansition = Value

Value = SCPI.STATus.QUEStionable.BLIMit.CHANnel(Ch).PTRansition

Description

This command sets/gets the value of the positive transition filter of the "Questionable Bandwidth Limit Channel Status Register" for the specified channel.

Variable

Parameter

Value

Description

The value of the positive transition filter of the Questionable Bandwidth Limit Channel Status Register

Data type

Long integer type (Long)

Range

0 to 65535

Preset value

Varies depending on the upper limit setting of the number of channels/traces.

Note

Bits 15 cannot be set to 1.

For information on the variable (Ch), see Ch.  

Examples

Dim Stat As Long
SCPI.STATus.QUEStionable.BLIMit.CHANnel(1).PTRansition = 0
Stat = SCPI.STATus.QUEStionable.BLIMit.CHANnel(1).PTRansition

Related objects

SCPI.STATus.QUEStionable.BLIMit.CHANnel(Ch).EVENt

SCPI.STATus.QUEStionable.BLIMit.CHANnel(Ch).NTRansition

Equivalent key

No equivalent key is available on the front panel.

Equivalent SCPI command

Syntax

:STATus:QUEStionable:BLIMit:CHANnel{[1]-160}:PTRansition <numeric>

:STATus:QUEStionable:BLIMit:CHANnel{[1]-160}:PTRansition?

Query response

{numeric}<newline><^END>

Example of use

10 OUTPUT 717;":STAT:QUES:BLIM:CHAN1:PTR 16"
20 OUTPUT 717;":STAT:QUES:BLIM:CHAN1:PTR?"
30 ENTER 717;A