Property (Read-only)
Value = SCPI.STATus.QUEStionable.LIMit.CONDition
This command reads the value of the Questionable Limit Status Condition Register.
Parameter |
Value |
Description |
Value of the Questionable Limit Status Condition Register |
Data type |
Long integer type (Long) |
Dim Stat As Long
Stat = SCPI.STATus.QUEStionable.LIMit.CONDition
SCPI.STATus.QUEStionable.LIMit.NTRansition
SCPI.STATus.QUEStionable.LIMit.PTRansition
No equivalent key is available on the front panel.
:STATus:QUEStionable:LIMit:CONDition?
{numeric}<newline><^END>
10 OUTPUT 717;":STAT:QUES:LIM:COND?"
20 ENTER 717;A