Property (Read-only)
Value = SCPI.STATus.QUEStionable.RLIMit.CHANnel(Ch).CONDition
This command reads the value of the Questionable Ripple Limit Channel Status Condition Register for the specified channel.
Parameter |
Value |
Description |
The value of the Questionable Ripple Limit Channel Status Condition Register. |
Data type |
Long integer type (Long) |
For information on the variable (Ch), see Ch.
Dim Stat As Long
Stat = SCPI.STATus.QUEStionable.RLIMit.CHANnel(1).CONDition
SCPI.STATus.QUEStionable.RLIMit.CHANnel(Ch).NTRansition
SCPI.STATus.QUEStionable.RLIMit.CHANnel(Ch).PTRansition
No equivalent key is available on the front panel.
:STATus:QUEStionable:RLIMit:CHANnel{[1]-160}:CONDition?
{numeric}<newline><^END>
10 OUTPUT 717;":STAT:QUES:RLIM:CHAN1:COND?"
20 ENTER 717;A