Property (Read-Write)
SCPI.STATus.QUEStionable.RLIMit.CHANnel(Ch).NTRansition = Value
Value = SCPI.STATus.QUEStionable.RLIMit.CHANnel(Ch).NTRansition
This command sets/gets the value of the negative transition filter of the Questionable Ripple Limit Channel Status Register for the specified channel.
Parameter |
Value |
Description |
The value of the negative transition filter of the Questionable Ripple Limit Channel Status Register. |
Data type |
Long integer type (Long) |
Range |
0 to 65535 |
Preset value |
0 |
Note |
Bits 15 cannot be set to 1. |
For information on the variable (Ch), see Ch.
Dim Stat As Long
SCPI.STATus.QUEStionable.RLIMit.CHANnel(1).NTRansition = 16
Stat = SCPI.STATus.QUEStionable.RLIMit.CHANnel(1).NTRansition
SCPI.STATus.QUEStionable.RLIMit.CHANnel(Ch).EVENt
SCPI.STATus.QUEStionable.RLIMit.CHANnel(Ch).PTRansition
No equivalent key is available on the front panel.
:STATus:QUEStionable:RLIMit:CHANnel{[1]-160}:NTRansition <numeric>
:STATus:QUEStionable:RLIMit:CHANnel{[1]-160}:NTRansition?
{numeric}<newline><^END>
10 OUTPUT 717;":STAT:QUES:RLIM:CHAN1:NTR 16"
20 OUTPUT 717;":STAT:QUES:RLIM:CHAN1:NTR?"
30 ENTER 717;A