Property (Read-only)
Ctlg = SCPI.SYSTem.COMMunicate.ECAL.CATalog
This command reads the ID string of ECal that are connected to the ENA through USB. Use the list to select an ECal.
|
Parameter |
Ctlg |
|
Description |
Returns a string containing the following parameters for all the connected ECals:
|
|
Data type |
Character string type (String) |
Dim Ctlg As String
Ctlg = SCPI.SYSTem.COMMunicate.ECAL.CATalog
SCPI.SYSTem.COMMunicate.ECAL.DEFine
No equivalent key is available on the front panel.
:SYSTem:COMMunicate:ECAL:CATalog
{string}<newline><^END>
10 OUTPUT 717;":SYSTem:COMMunicate:ECAL:CATalog?"
20 ENTER 717;A$