Property (Read-Write)
SCPI.SYSTem.COMMunicate.ECAL.DEFine = ECalId
ECalId = SCPI.SYSTem.COMMunicate.ECAL.DEFine
This command sets/gets the ID string of the ECal being used at that time.
|
Parameter |
ECalId |
|
Description |
Returns ECalId string containing the following parameters:
|
|
Data type |
Character string type (String) |
Dim ECal As String, ECalReturn As String
SCPI.SYSTem.COMMunicate.ECAL.DEFine = "N4431B 03605"
ECalReturn = SCPI.SYSTem.COMMunicate.ECAL.DEFine
SCPI.SYSTem.COMMunicate.ECAL.CATalog
Cal > ECal > ECal
:SYSTem:COMMunicate:ECAL:DEFine <string>
:SYSTem:COMMunicate:ECAL:DEFine?
{string}<newline><^END>
10 OUTPUT 717;":SYSTem:COMMunicate:ECAL:DEFine ""N4431B 03605"""
10 OUTPUT 717;":SYSTem:COMMunicate:ECAL:DEFine?"
20 ENTER 717;A$