Scalar-Mixer Calibration

Other topics about Performing Calibration

Overview

The E5072A's frequency offset function allows you to measure any device that has different input and output frequencies. To correct such measurements, you must determine the transmission frequency characteristics at different frequencies.

Scalar-mixer calibration is a method to calculate the transmission frequency characteristics at different frequencies by using a power meter.

Measurement of Scalar-Mixer Calibration Data

Setting Frequency Offset Function

You can use the following command to enable the frequency offset function before starting a measurement of scalar-mixer calibration data.

:SENS{1-160}:OFFS

Selecting Calibration Port and Type

You can use the following commands to set the port on which a measurement of scalar-mixer calibration data is implemented and as well as the type of calibration.

"SMIX2" will set a scalar-mixer calibration for 2-port forward, reverse and both directions. "SOLT1" will set 1-port calibration.

The setting of forward, reverse and both directions is not dependent on the order of the two specified ports but determined by specifying an appropriate command for calibration data measurement, such as

 :SENS{1-160}:CORR:OFFS:COLL:OPEN

Measuring the Calibration Data

You can use the following command to measure the scalar-mixer calibration data.

Measuring Power

You can use the following command to measure power.

:SENS{1-36}:CORR:OFFS:COLL:PMET

Calculation of scalar-mixer calibration coefficient

If the needed measurement is completed for the calibration port and type you have selected, use the following command to start calculation of calibration coefficients.

:SENS{1-160}:CORR:OFFS:COLL:SAVE

Turning ON/OFF scalar-mixer error correction

To turn ON or OFF scalar-mixer error correction, use the following command. This command is commonly used for the normal calibration; scalar-mixer calibration data are enabled while the frequency offset is turned ON, and the normal calibration data are enabled while it is turned OFF.

:SENS{1-160}:CORR:STAT

Implementing scalar-mixer calibration with ECal

An ECal (Electronic Calibration) module allows you to perform scalar-mixer calibration and 1-port calibration without needing to replace the standard device.

To perform ECal, use one of the following commands:

Calibration type

Command

1-Port Calibration

:SENS{1-160}:CORR:OFFS:COLL:ECAL:SOLT1

Scalar-Mixer Calibration

:SENS{1-160}:CORR:OFFS:COLL:ECAL:SMIX2

Simply issuing one of the above commands completes some of the tasks necessary for error correction, including measuring the calibration data, calculating the calibration coefficients, and running the error correction feature. To implement scalar-mixer calibration, you must measure the power in advance. For 1-port calibration, you do not need to do this.